KAS Breakdown

Domains Concept (Technology) Task (Tools) Reference
HMI
  Kollmorgen Visualization Builder
Add an HMI
HMI
Controllers – AKD PDMMPCMM
Programmable Drive Multi-axis Master Add Controller

Configure Controller
Controller
PLC
PLC
IEC 61131-3 ST editor
IL editor
FBD editor
FFLD editor
SFC editor
 
Variable dictionary
Softscope
ST Language
IL Language
FBD Language
FFLD Language
SFC Language
Motion Engine
Motion
Motion Concept
Pipe Network
Design Pipe Network
Pipe Network Editor
Create Cam Profile
Cam Profile Editor
Softscope
 
PLCopen
Fieldbus
Fieldbus
EtherCAT Configure EtherCAT Motion Bus Motion bus
Cables
I/O Terminal
I/O Modules
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs Add I/O terminal
I/O mapping to variable
Remote Input/Output (I/O Terminals)

Drive
Drive

 
AKD
AKD2G
AKD-C
AKD-N
S300
S700
Add and configure drive
Drive Configuration
AKD Firmware Download
AKD
Motor
Motor
Kollmorgen Servomotor   AKM
AKM2G
Mechanical
Mechanical
    Linear Positioners
Gearheads

Table 2-1: KAS - Technologies and Tools